MPC5743R Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5743R Interrupt

2,085件の閲覧回数
hongpingxu-b364
NXP Employee
NXP Employee

MPC5743R default booting core is core1, not core 0. So, need clear understanding on multicore logic, and how to enable different core

a) The actual core id is read by “uint16_t coreId = GetCoreID ();” in InitINTC.

b) The interrupt configuration shall base on coreid, not hardcode “INTC_0.PSR[226].R= 0x4001; /* IRQ sent to Core 1, Priority 1 */”

c) The macro shall be enabled based on core id, TURN_ON_CPU1

A quick test code is as attached, move all configuration to core 1, and interrupt works well.

IDE: S32DS for Power version: 2017r1 with Update 10.

1 返信

1,961件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

MPC5743R default booting core is core1, not core 0.

Yes, this is correct. No matter of micro version the boot  core is always core 1 which is only core capable of BAF execution.

So, need clear understanding on multicore logic, and how to enable different core

This is described in reference manual:

In short -

1. program CORE0 Control (MC_ME_CCTL1) register to enable core for target modes

2. program CORE0 Address (MC_ME_CADDR1) with RMC bit set

3. perform mode transition to desired mode

second option is:

Enable the core0 and set his boot address in RCHW, and it will be active after reset directly.

regards,

Peter

0 件の賞賛
返信