MPC56XX link error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC56XX link error

2,308 Views
384753860
Contributor I

IDE is codewarrior 10.5.  Processor is MPC5644A.

 

Errors(3 item)
Linked failed.
Linker command faile output section '.ivor_branch_table' has a type or input which is incompatible with section '.ivor_branch_table' in file 'C:\workspace\w20\FLASH\ivor_branch_table_c.obj'. Change the type or add an input for this.
mingw32-make:***[w20_prj.elf] Error 1

 

Wating for ideas. 

Thank you very much.

Labels (1)
0 Kudos
Reply
2 Replies

1,947 Views
stanish
NXP Employee
NXP Employee
0 Kudos
Reply

1,961 Views
lizhichaosdut
Contributor III

I met thesame error,how to solve this ?

0 Kudos
Reply