MPC5675K development Kit Details

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5675K development Kit Details

2,884 Views
mithunp_s
Contributor III

Hi All,

 

One of my customer has chosen MPC5675 and want to buy the development kit for the same.

 

 

MPC567xKEVB Product Summary Page

 

Below link has two related development details but we want to know the difference between the two parts

 

 

Hardware / Software / Tech Support Bundle MPC5675KEVB257 Evaluation Board

 

 

&

 

 

Hardware Only MPC5675KEVB473 Evaluation Board\

 

Regards

Mithun

Labels (1)
0 Kudos
Reply
2 Replies

2,515 Views
Martin35804
NXP Employee
NXP Employee

MPC5675KEVB257/473 Evaluation Kit comes with P&E's USB QORIVVA MPC55xx/56xx MULTILINK (the blue one).

Use the links below as a reference.
http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320021

MPC5675K family is offered in a 257MAPBGA and 473MAPBGA package. Both the 473MAPBGA and 257BGA packages support Nexus debug for development purposes.

The main difference between MPC5675KEVB257/473 Evaluation Kits is that the DDR PISMO connector has been removed from the 257BGA and the jumper numbering is different. Otherwise the content of the package is the same.

2,515 Views
matthewclark
Contributor III

Martin,

What's the default clock speed for the MPC5675K on the EVB 473 running in LSM?  I've not fiddled with the jumpers, but can't quite find in the docs what processor runs at by default.  Thanks.

Matt

0 Kudos
Reply