MPC5674F: pins for serial boot mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5674F: pins for serial boot mode

ソリューションへジャンプ
803件の閲覧回数
matthiasgeipel
Contributor I

Hello,

 

can somebody please specify in detail, at which pins of the MPC5674F the serial boot mode is available for eSCI and FlexCAN?

TXDA/RXDA and CNTXA/CNRXA are available at several pins, but I suppose the device will use only one pair each. Is it TXDA_GPIO89/RXDA_GPIO90 for eSCI and CNTXA_TXDA_GPIO83/CNRXA_RXDA_GPIO84 for FlexCAN?

ラベル(1)
0 件の賞賛
返信
1 解決策
689件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

you are right. Pins 89 and 90 are used for eSCI, pins 83 and 84 are used for CAN. In other words - if the functions are available at several pins then "primary" pins are used. Notice that this is hard-coded, there's no way to select other pair of pins for serial boot.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
690件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

you are right. Pins 89 and 90 are used for eSCI, pins 83 and 84 are used for CAN. In other words - if the functions are available at several pins then "primary" pins are used. Notice that this is hard-coded, there's no way to select other pair of pins for serial boot.

Regards,

Lukas

0 件の賞賛
返信