MPC5674F: pins for serial boot mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5674F: pins for serial boot mode

Jump to solution
616 Views
matthiasgeipel
Contributor I

Hello,

 

can somebody please specify in detail, at which pins of the MPC5674F the serial boot mode is available for eSCI and FlexCAN?

TXDA/RXDA and CNTXA/CNRXA are available at several pins, but I suppose the device will use only one pair each. Is it TXDA_GPIO89/RXDA_GPIO90 for eSCI and CNTXA_TXDA_GPIO83/CNRXA_RXDA_GPIO84 for FlexCAN?

Labels (1)
0 Kudos
1 Solution
502 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

you are right. Pins 89 and 90 are used for eSCI, pins 83 and 84 are used for CAN. In other words - if the functions are available at several pins then "primary" pins are used. Notice that this is hard-coded, there's no way to select other pair of pins for serial boot.

Regards,

Lukas

View solution in original post

0 Kudos
1 Reply
503 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

you are right. Pins 89 and 90 are used for eSCI, pins 83 and 84 are used for CAN. In other words - if the functions are available at several pins then "primary" pins are used. Notice that this is hard-coded, there's no way to select other pair of pins for serial boot.

Regards,

Lukas

0 Kudos