Hello,
can somebody please specify in detail, at which pins of the MPC5674F the serial boot mode is available for eSCI and FlexCAN?
TXDA/RXDA and CNTXA/CNRXA are available at several pins, but I suppose the device will use only one pair each. Is it TXDA_GPIO89/RXDA_GPIO90 for eSCI and CNTXA_TXDA_GPIO83/CNRXA_RXDA_GPIO84 for FlexCAN?
Solved! Go to Solution.
Hi,
you are right. Pins 89 and 90 are used for eSCI, pins 83 and 84 are used for CAN. In other words - if the functions are available at several pins then "primary" pins are used. Notice that this is hard-coded, there's no way to select other pair of pins for serial boot.
Regards,
Lukas
Hi,
you are right. Pins 89 and 90 are used for eSCI, pins 83 and 84 are used for CAN. In other words - if the functions are available at several pins then "primary" pins are used. Notice that this is hard-coded, there's no way to select other pair of pins for serial boot.
Regards,
Lukas