MPC5674F Includes eTPU or eTPU2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5674F Includes eTPU or eTPU2?

Jump to solution
6,928 Views
erdinc26
Contributor II

Hello,

I work with SPC5674FK0MVY3 microcontroller. When I look MPC5674RM_Rev7 in page 1-3, there is a sentence after table of comparison "eTPU2 only available on revision 2 release of device."

Then I find my revision from my number of microcontroller "SPC5674FK--0--MVY3" . According to datasheet my revision is 0.

Until this time I thought working on eTPU2. How can I be sure? 

Also I have a development board. On this board I have "SPC5674FMVY3", but there is no revision number in this part. (If other additional information is important here there 3M17W, QCG1805G)

I need a solution for the uncertainty.

Best regards,

Erdinc

 

#mpc5674f @johndiener 

 

0 Kudos
Reply
1 Solution
6,790 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport
  1. Is there a microcontroller belonging to the MPC5674F series that is not eTPU2 (eTPU only)?

- Rev 1, but has been only pre-production device, customers should not get in contact with such devices. This is mature product for long time.

  1. Model SPC5674FAMVY3 is also included in the datasheet. But how will I find out about this mask without buying it?

- It is either mask 3M17W or 0N31E (without further specification), in both case chip revision 2.3.

  1. Is there a list where I can access this mask information you have? Because I don't have the product and I want to buy it, but I can't be sure about the mask identifiers. When I go to purchasing sites, only the part number is written. I need detailed information here, but I could not find such content on NXP's website.

- There is lot of options for this device, ordering part you may find on our web and mostly they do have mask identifier included in ordering number.

davidtosenovjan_0-1721814820274.png

 

  1. Should I get technical support every time I need revision information?

- I don't think it is necessary every time, but in case of confusion you can contact us, we are here for you.

View solution in original post

7 Replies
6,816 Views
erdinc26
Contributor II

Firstly, thank you for your reply.
I have a few more questions.

  1. Is there a microcontroller belonging to the MPC5674F series that is not eTPU2 (eTPU only)?
  2. Model SPC5674FAMVY3 is also included in the datasheet. But how will I find out about this mask without buying it?
  3. Is there a list where I can access this mask information you have? Because I don't have the product and I want to buy it, but I can't be sure about the mask identifiers. When I go to purchasing sites, only the part number is written. I need detailed information here, but I could not find such content on NXP's website.
  4. Should I get technical support every time I need revision information?

Best regards

Erdinc

0 Kudos
Reply
6,791 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport
  1. Is there a microcontroller belonging to the MPC5674F series that is not eTPU2 (eTPU only)?

- Rev 1, but has been only pre-production device, customers should not get in contact with such devices. This is mature product for long time.

  1. Model SPC5674FAMVY3 is also included in the datasheet. But how will I find out about this mask without buying it?

- It is either mask 3M17W or 0N31E (without further specification), in both case chip revision 2.3.

  1. Is there a list where I can access this mask information you have? Because I don't have the product and I want to buy it, but I can't be sure about the mask identifiers. When I go to purchasing sites, only the part number is written. I need detailed information here, but I could not find such content on NXP's website.

- There is lot of options for this device, ordering part you may find on our web and mostly they do have mask identifier included in ordering number.

davidtosenovjan_0-1721814820274.png

 

  1. Should I get technical support every time I need revision information?

- I don't think it is necessary every time, but in case of confusion you can contact us, we are here for you.

6,845 Views
erdinc26
Contributor II

In MPC5674F Datasheet , page 3 "Table 1. Orderable Part Numbers", there are 18 part numbers.

Can you share revision list for them? @davidtosenovjan 

0 Kudos
Reply
6,830 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

mask => Revison
2M17W => 2.2
3M17W => 2.3
0N31E => 2.3

3M17W and 0N31E differs in manufacturing facility.

What is stated in DS, in somehow weirdly described, I will report it as documentation error as

"Revision of Silicon
3 = Rev 3 (ATMC)
0 = Rev 0 (TSMC14)"

because Rev 0 as stated here is actually latest one.

 

6,888 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

'F3' and 'K0' are mask identifiers.

SPC5674FK0MVY3 is mask 0N31E. Your second device is mask 3M17W.

Both are equivalent and both chips are revison 2 thus included eTPU2 module.

6,884 Views
erdinc26
Contributor II
Thanks for answer.
How do you determine of revision of these microcontollers? Do you have any link?
0 Kudos
Reply
6,889 Views
erdinc26
Contributor II

@davidtosenovjan 

Can you help me? 

0 Kudos
Reply