MPC5674F Bootload

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5674F Bootload

3,542件の閲覧回数
pyi285
Contributor II

Can someone explain me the code or method to bootloader the MPC5674F chip?

The chip I have is SPC5674FMVVS chip

 

#MPC5674F #bootloader #SPC5674

0 件の賞賛
返信
4 返答(返信)

3,531件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @pyi285 

We provide Rappid bootloader which can use either UART or CAN (per release notes - only UART in case of MPC5674F). It uses BAM serial boot mode. Notice that we do not provide source codes, it cannot be modified:

https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&appType=license

To start this bootloader, it is necessary to reconfigure BOOTCFG pins in order to start BAM serial download. If it is not suitable for your application, it’s necessary to use flash resident bootloader.

 

If you are interested in flash resident bootloader, attached is a draft of application note:

https://community.nxp.com/servlet/JiveServlet/download/427962-1-279359/bootloader.zip

It’s written directly for MPC5634M, software is working. It can be used as a starting point to develop own solution. It’s necessary to use these SSD flash drivers:

http://www.nxp.com/lgfiles/Qorivva/MPC5674F_C90FL_SSD_DRV.exe

 

Just in case, this is updated and published version for MPC57xx devices (software is written for MPC5748G):

http://www.nxp.com/assets/documents/data/en/application-notes/AN5319.pdf

http://www.nxp.com/assets/documents/data/en/application-notes-software/AN5319SW.zip

 

And if you are looking for out of box solution, you can ask Vector (or other SW vendors) for help:

https://www.vector.com/int/en/products/products-a-z/embedded-components/flash-bootloader#

Regards,

Lukas

0 件の賞賛
返信

3,431件の閲覧回数
pyi285
Contributor II

Can you write the Bootloader code used with the SPC5674FF3MVV3 Chip?

0 件の賞賛
返信

3,425件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

This is not a service provided by our free online technical support. You can request a solution from our paid engineering services:

https://www.nxp.com/support/support/nxp-engineering-services:SW-SUPPORT

Regards,

Lukas

0 件の賞賛
返信

3,365件の閲覧回数
pyi285
Contributor II
I am sorry But I don't have enough time, so I need a quick answer and an accurate code. I urgently need a bootloader code related to the MPC5674F chip I am using.
If you can't write the code, can you elaborate on the address or register that needs to be changed?
please i need a lot

It is difficult to understand the present
0 件の賞賛
返信