MPC5646C BAM with external clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5646C BAM with external clock

跳至解决方案
2,675 次查看
tbonkers
Contributor III

I have a MPC5646C mounted on a PCB and using an external clock (no crystal oscillator). The reference manual for the processor mentions that BAM uses 4-40 MHz external crystal oscillator. Does that mean I will not be able to invoke it, as my processor does not use a crystal?

0 项奖励
回复
1 解答
2,629 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hmm,

I expect this is not the case as I read in Manual that BAM initialize the XOSC, so BAM must be running from IRC in that time. It also would not be safe in case of loss of XOSC, the device must run from IRC.

petervlna_1-1640595754827.png

Best regards,

Peter

 

 

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,593 次查看
tbonkers
Contributor III

Managed to invoke the BAM on a board which uses a 40 MHz external clock. The baud rate is 48000 - checked it with the logic analyzer. However the RAppID does not have an option for baud 48000 - is there a way to add it to the menu?

 

0 项奖励
回复
2,583 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Well, I do not use any kind of configuration tools like Rappid due to its limitation.

But if you have any questions on it you can drop a email here: [email protected] which is direct rappid support.

Best regards,

Peter

2,630 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hmm,

I expect this is not the case as I read in Manual that BAM initialize the XOSC, so BAM must be running from IRC in that time. It also would not be safe in case of loss of XOSC, the device must run from IRC.

petervlna_1-1640595754827.png

Best regards,

Peter

 

 

 

0 项奖励
回复
2,614 次查看
tbonkers
Contributor III

What you point out makes sense, probably I am doing something wrong and can't start the BAM.

0 项奖励
回复