MPC5645S eMIOS_SAIC problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5645S eMIOS_SAIC problem

Jump to solution
3,048 Views
weiguoyan
Contributor II

Hi,

I am using the MPC5645S. I use the channel 20 and channel 21 of  the eMIOS1 with SAIC  mode. Two channels register configuration  and initialize  are the same. but the channel 21 can capture the input  frequency signal and enter the interrupt .The channel 20 can't enter the interrupt. 

who can help me to solve this problem.   

Thanks!

 

void EMIOS1Init(void)
{
EMIOS_1.MCR.B.GPRE = 255; // 64M/256=250kHz
EMIOS_1.MCR.B.GPREN = 1; 
EMIOS_1.MCR.B.FRZ = 1; 
}// end of EMIOS1Init

 

void CounterBusAInit(void)
{
EMIOS_1.CH[23].CADR.R = 0xFFFF;
EMIOS_1.CH[23].CCR.B.MODE = 0x50; 
EMIOS_1.CH[23].CCR.B.BSL = 0x3; 
EMIOS_1.CH[23].CCR.B.UCPRE = 0x1; // 250k/2 =125kHz
EMIOS_1.CH[23].CCR.B.UCPEN = 1;
EMIOS_1.CH[23].CCR.B.FREN = 1;
EMIOS_1.CH[23].CCR.B.FEN = 1;
}// end of CounterBusAInit

 

void ICInit(void)
{
UBYTE i;
SIU.PCR[PF1].R = 0x0500; // EMIOS1-20
SIU.PCR[PF3].R = 0x0500; // EMIOS1-21
EMIOS1Init(); 
for( i=20;i<22;i++ )
{
EMIOS_1.CH[i].CCR.B.MODE = 0x02; // SAIC mode
EMIOS_1.CH[i].CCR.B.BSL = 0x00; 
EMIOS_1.CH[i].CCR.B.IF = 0x02;
EMIOS_1.CH[i].CCR.B.FCK = 1;
EMIOS_1.CH[i].CCR.B.FEN = 1;
EMIOS_1.CH[i].CCR.B.DMA = 0; 
EMIOS_1.CH[i].CCR.B.EDSEL = 0; 
EMIOS_1.CH[i].CCR.B.EDPOL = 1; 
EMIOS_1.CH[i].CCR.B.UCPRE = 0; 
EMIOS_1.CH[i].CCR.B.UCPEN = 1; 
EMIOS_1.CH[i].CCR.B.FREN = 1; 
}
CounterBusAInit(); 
INTC_InstallINTCInterruptHandler(ISR_SAIC20,169,3);
INTC_InstallINTCInterruptHandler(ISR_SAIC21,170,3);
INTC_InstallINTCInterruptHandler(ISR_EMIOS123OVFL,172,3);
}// end of ICInit

Labels (1)
1 Solution
2,862 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

You have to route the pin PF1 to eMIOS1[20] with the help of SIU.PSMI register. See table 43-14 of the RM and set PSMI[44]=1.

 

BR, Petr

View solution in original post

3 Replies
2,863 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

You have to route the pin PF1 to eMIOS1[20] with the help of SIU.PSMI register. See table 43-14 of the RM and set PSMI[44]=1.

 

BR, Petr

2,862 Views
weiguoyan
Contributor II

Thank you for your answer. 

The problem is resolved.

Best wishes!

0 Kudos
Reply
2,862 Views
weiguoyan
Contributor II

Thank you for your answer. The problem is resolved.

Best wishes!

0 Kudos
Reply