[MPC5645S] Display 16bpp image using external flash memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MPC5645S] Display 16bpp image using external flash memory

950 Views
josepgorgues
Contributor II

Hello,

 

I'm Working with MPC5645S and code warrior IDE 5.9.

Following the document "AN4865". I have the DCU3 configured and running with a TFT of 800x480 using a Nominal clock of 32MHz.

We display correctly small images (size: 16x6 pixels) from the External memory.

Unfortunately when we use a image that have for example 300x300 pixels, this image was not read correctly.

To read these images I use the "AHB address" to set the beginning address of layer data. (DCU.LAYER[6].CTRLDESCL3.R = 0x70000000)

 

Please, could somebody help me with this problem?

 

Thanks,

Josep Gorgues

Labels (1)
0 Kudos
Reply
0 Replies