[MPC5645S] Display 16bpp image using external flash memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[MPC5645S] Display 16bpp image using external flash memory

948件の閲覧回数
josepgorgues
Contributor II

Hello,

 

I'm Working with MPC5645S and code warrior IDE 5.9.

Following the document "AN4865". I have the DCU3 configured and running with a TFT of 800x480 using a Nominal clock of 32MHz.

We display correctly small images (size: 16x6 pixels) from the External memory.

Unfortunately when we use a image that have for example 300x300 pixels, this image was not read correctly.

To read these images I use the "AHB address" to set the beginning address of layer data. (DCU.LAYER[6].CTRLDESCL3.R = 0x70000000)

 

Please, could somebody help me with this problem?

 

Thanks,

Josep Gorgues

ラベル(1)
0 件の賞賛
返信
0 返答(返信)