MPC5644B FLEXCAN module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5644B FLEXCAN module

2,197 次查看
muhammadrafique
Contributor I


Hi All,

 

I have MPC5644B and i am using Flexcan 0 on it.The problem i am facing is that after transmitting first frame,Flexcan dosen't transmit any other frame. The CAN module is receiving frames just fine?

Thanks in advance for help.

标签 (1)
0 项奖励
回复
3 回复数

2,015 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm not sure what's wrong when reading this short description but I can provide very simple example that works as expected. It just sends data from CAN0 to CAN1 and everything is working as expected. See please attachment.

Regards,

Lukas

0 项奖励
回复

2,015 次查看
eunjolee
Contributor I

Thank you very much.

Eunjo Lee

0 项奖励
回复

2,015 次查看
gurumurthykola
Contributor I

Hi All,

I also faced the same issue in FlexCAN module of MPC5777C controller. It is transmitting only one CAN frame. after that the FlexCAN is put into Freeze Mode. It is happening with Receive also. After receive one frame the FlexCAN module is put into Freeze mode.

Please help anybody.

Thanks in advance.

Regards,

Gurumurthy K

0 项奖励
回复