MPC5643L non correctable SRAM errors observability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5643L non correctable SRAM errors observability

Jump to solution
3,264 Views
stefanodimasci1
Contributor III

In this kind of the device a non correctable error causes a reset. I'd like to know by software and send to the outside world (using the UART) what happened and where. The problem is that after the reset , as the main start, every information is lost in ESR. When should I record the information to let the software know that the reset was caused by a non correctable error in SRAM?

Labels (1)
1 Solution
3,052 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, that’s right. I have mentioned it in chapter 7.1 §3

You can keep ESCM reporting disabled. In this case multi-bit ECC error device is not reset and you can handle ECC error in IVOR1 exception (see chapter 5.1) but such approach does not catch ECC errors from other masters than the core.

It is such specialty of MPC5643L device.

View solution in original post

6 Replies
3,052 Views
stefanodimasci1
Contributor III

If I access a SRAM or flash location with a non correctable error in such way:

value=*((uint32_t *)0x40000000)

will it be recorded in the core without ECSM reporting?

Thank you

3,052 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it'll be.

3,052 Views
stefanodimasci1
Contributor III

Ok,

but the problem now is: how can i check if my handling is correct If I can inject a fault just with ECSM reporting enabled?

Thank you very much

0 Kudos
Reply
3,052 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have described the topic in section 7 in following document. You can find in here:

AN5200 - Error Correcting Codes Implemented on MPC55xx and MPC56xx

3,052 Views
stefanodimasci1
Contributor III

Thank you very much, I've already read that.

But the problem is: after the reset ESR is set to all 0s,so I can't access ECC registers to know what happened (that would cause an error), even if I know from RGM that an ECC error happened. I don't see how can I have information about the problem in this way

3,053 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, that’s right. I have mentioned it in chapter 7.1 §3

You can keep ESCM reporting disabled. In this case multi-bit ECC error device is not reset and you can handle ECC error in IVOR1 exception (see chapter 5.1) but such approach does not catch ECC errors from other masters than the core.

It is such specialty of MPC5643L device.