MPC5634M FlexCAN Individual Rx Mask Register Can not write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5634M FlexCAN Individual Rx Mask Register Can not write

1,869 Views
413515651
Contributor I

 I do that:

CAN_A.MCR.B.MBFEN =1; //Use Individual Rx Mask Register

CAN_A.RXIMR[4].B.MI = 0x00001000;

but:CAN_A.RXIMR[4].R  is Always Read 0x00000000;

1.bmp

2.bmp

MPC5634M datasheet

3.bmp

0 Kudos
Reply
2 Replies

1,640 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

The Individual Rx Mask Registers can only be accessed by the CPU while the module is in Freeze Mode and MBFEN is set. Out of Freeze Mode, write accesses are blocked and read accesses will return “all zeros”.

So be sure the FlexCAN is allowed to enter Freeze mode (MCR[FRZ] set) and Freeze mode is really entered once you break debugger (FRZACK and NOTRDY flags set).

BR, Petr

1,640 Views
413515651
Contributor I

Thank you!! I solved it.

0 Kudos
Reply