MPC5634 eTpu function Loss synchronization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5634 eTpu function Loss synchronization

1,229件の閲覧回数
Jasting
Contributor II

Synchronous loss in steady engine operation.

When I check "*cpba_tooth_period_log" in “crank_instance_t",I foung some member become very small。

Jasting_0-1729664856188.png

The experimental results are as follows.While running, etpu_tooth_period_log[80] suddenly drops from 33800 to 21800.And crank states err occur.The rest of the etpu tooth period log(log[0],log[40],log[119],) data looks normal.

Jasting_1-1729665420661.png

I checked the input crankshaft original signal and there was no signal anomaly when the fault occurred.I tested the duration of the first 1 and 2 teeth of the failure,They all last around 820us.

Jasting_2-1729666089411.png

Here are some of my eTPU parameter matching values

Jasting_3-1729666415763.png

So how can I find the cause of the problem? Thank you very much!

 

タグ(3)
0 件の賞賛
返信
1 返信

1,210件の閲覧回数
Jasting
Contributor II

My Crank config is as follows:

Jasting_0-1729756132491.png

 

0 件の賞賛
返信