MPC5606B : Inbuilt NVM memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5606B : Inbuilt NVM memory

1,459 Views
anithaa
Contributor I

Hello,

 

Does MPC5606B has inbuilt NVM area where we could store and write NVM related data? If yes how could we use it, its configuration,size,application notes etc?

 

Many thanks for the assistance.

 

Regards,

Anitha

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,341 Views
martin_kovar
NXP Employee
NXP Employee

Hello Anitha,

MPC5606B has not independent NV memory. MPC has Code and Data flash which are non-volatile and SRAM which is volatile. About using and configuration flash memory please look at the reference manual chapter 30.

http://cache.freescale.com/files/32bit/doc/ref_manual/MPC5607BRM.pdf?fsrch=1&sr=1&pageNum=1

For working with flash memory you can also use flash standard software driver which you can find here:

MPC560xB|32-bit MCU|Body-Electronic|Freescale

Regards,

Martin

0 Kudos
Reply