MPC5606B Configure variable in RAM to run

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5606B Configure variable in RAM to run

3,305 次查看
明伟张
Contributor III

firstly,the global variable are configured to flash address which i defined; i hope the variable copy to RAM address which i defined when workspace start running;

can offer me sample code?

 

thanks!

标签 (1)
0 项奖励
回复
6 回复数

2,965 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

here is the example:

In linker file I added myROM and myRAM segment:

MEMORY

{

    resetvector:           org = 0x00000000,   len = 0x00000008

    init:                   org = 0x00000020,   len = 0x00000FE0   

    exception_handlers:    org = 0x00001000,   len = 0x00001000

    internal_flash:        org = 0x00002000,   len = 0x000FD000

   

    myROM:                     org = 0x000FF000,   len = 0x00001000

   

    internal_ram:          org = 0x40000000,   len = 0x00011000

   

    myRAM:                       org = 0x40011000,   len = 0x00001000

   

    heap  :                org = 0x40012000,   len = 0x00001000

    stack :                org = 0x40013000,   len = 0x00001000

}

Then use this syntax in SECTION:

SECTIONS

{

...

.myRAM BIND(ADDR(myRAM)) LOAD (ADDR(myROM)): {} > myRAM

...

}

And then in *.c file:

#pragma push

#pragma section sdata_type ".myRAM" ".myRAM"

unsigned int my_var1 = 0x11223344;

unsigned int my_var2 = 0xAABBCCDD;

unsigned int my_var3 = 0x55556666;

#pragma pop

The initial values will be copied during startup from myROM to variables in myRAM.

Regards,

Lukas

0 项奖励
回复

2,965 次查看
明伟张
Contributor III

the two question is not  same! In fact,for exampel:

i define a variable in flash as follow:

MEMORY

{

...

my_flash:   org = 0x003FF000,   len = 0x00001000

...

}

SECTIONS

{

...

.__my_flash LOAD (0x003FF000): {} > my_flash

...

}

In *.c file:

#pragma push

#pragma section all_types ".__my_flash" ".__my_flash "

uint32_t test = 0x1234;

#pragma pop

if it is OK,i want the variable "test" initial values can be copied during startup from my_flash to variables in myRAM.

so how to configure the myRAM in  *.c file:?? thanks! can offer me a sample code?

thanks verry verry much!!!!

0 项奖励
回复

2,965 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

you have to do it exactly in the same way as I showed in my previous post if you want to have variable in RAM that is initialized during startup.

The above can be used only for constant in flash.

Regards,

Lukas

0 项奖励
回复

2,965 次查看
明伟张
Contributor III

Hi,

I know,thanks.

but i also have a question,the variable is configured in Flash,i want the variable copy to ram address which i defined before MCU run?

0 项奖励
回复

2,965 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

that's what it does. In the example above, the startup files will copy the initial values stored in myROM to myRAM.

Lukas

0 项奖励
回复

2,965 次查看
明伟张
Contributor III

thanks! the problem is OK!

0 项奖励
回复