MPC5604S LCD without DCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5604S LCD without DCU

1,750 次查看
akhilprasad
Contributor III

I am using MPC5604S. I need to use LCD module to display the temperature. Should I enable DCU module ? will it work alone with LCD module ? Can anyone share a sample code for MPC5604S for LCD module without using DCU module.

0 项奖励
回复
3 回复数

1,504 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

If you mean MPC5606S's module called 'LCD Driver', it is for driving monochromatic segment display like for instance this one:
https://en.wikipedia.org/wiki/Twisted_nematic_field_effect

For driving TFT displays, DCU module in needed to use. I have example code for TFT display (i.e. DCU) that is present on MPC5606S-DEMO-V2 showing temperature measured with external temperature sensor:
https://community.nxp.com/docs/DOC-331807

0 项奖励
回复

1,504 次查看
akhilprasad
Contributor III

ok... thanks

0 项奖励
回复

1,504 次查看
akhilprasad
Contributor III

I have configured LCD module in MPC5604s. When I am connecing the LCD segment pins to CRO I could find a slow rise in the output signal. why is it so and can you suggest any method to rectify this issue.I have configured the port as special function and Pull up enabled, Am I missing any port configuration ? 

0 项奖励
回复