MPC5604EEVB64 Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5604EEVB64 Problem

1,161 Views
yankuang1
Contributor III

My board can not be properly debugged,the specific problem is described below:

After the board is powered by 12v, the status of the board is shown in the following figure

pastedImage_1.png

But after connecting the  MULTLINK, it becomes the following state,the D3  is on.

pastedImage_3.png

The DEBUG window is shown below

pastedImage_4.png

pastedImage_5.png

pastedImage_6.png

0 Kudos
Reply
1 Reply

1,085 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

1) Please check debugger cable and cable polarity (seems to be correct, but just to make sure).

2) Does the debugger have JP10 jumper which provides power supply? If yes, please disconnect this jumper.

3) Could you please the debugger with different board or this board with different debugger?

4) Have you ever been able to connect to the board? If yes, what did you load to memory?

Regards,

Martin

0 Kudos
Reply