MPC5604E fNET Stack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5604E fNET Stack

2,068 Views
suhass
Contributor II

Hi,

I'm working on MPC5604E and using its Fast Ethernet Controller[FEC], How to initialize fNET stack on the controller ?

 

Thanks & Regards

SUHAS S

Labels (1)
Tags (3)
2 Replies

1,904 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

please look at the following app note. There is good description of TCP/IP stack. App note is written for MPC5644B, but it is also usable for MPC5604E, because FEC module is the same.

http://cache.nxp.com/files/32bit/doc/app_note/AN4577.pdf?fsrch=1&sr=1&pageNum=1 

There are also software examples for this app note:

http://cache.nxp.com/files/32bit/doc/app_note/AN4577SW.zip 

Regards,

Martin

1,904 Views
suhass
Contributor II

Thanks for the reply Martin,

But according to "FNET Embedded TCP/IP Stack", MPC5604E is not supported. [Refer the attached Image]fnet.PNG

0 Kudos
Reply