MPC5604C NVUSRO Register Options

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5604C NVUSRO Register Options

1,676件の閲覧回数
ghogg
Contributor I

Hello everyone,

 

Please could someone give a detailed explanation regarding the OSCILLATOR_MARGIN and PAD3V5V options in present in the MPC5604C NVUSRO register?

 

Many thanks for the support.

 

Kind regards,

Greg

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,483件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

PAD3V5V pin determines length of the edges for output drive pads to keep the rise time the same for a 3V configuration and 5V configuration.

The OSCILLATOR MARGIN bit is provided for adjusting oscillation margin at higher frequencies.

It is recommended that OSCILLATOR_MARGIN = 0 for 4MHz and OSCILLATOR_MARGIN = 1 for 8MHz, 10MHz, 12MHz, 16MHz  frequencies.

Both bits are basically specifies drive strength of these pads.

0 件の賞賛
返信

1,483件の閲覧回数
kiminkim
NXP Employee
NXP Employee

Should we configure the PAD3V5V = 0 if when operating VDD is 5V?

0 件の賞賛
返信

1,483件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, you should. It'll work in both cases, but some electrical characteristic may not be fulfilled.

Expected configuration is either

VDD = 5.0 V ± 10%, PAD3V5V = 0

or

VDD = 3.3 V ± 10%, PAD3V5V = 1

0 件の賞賛
返信