MPC5604 not to ADC interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5604 not to ADC interrupt

991 Views
崔亚飞
Contributor II

I recently used in the MPC5604 ADC interrupt function, found that it can not get into the interrupt, the initial configuration no problem, and finally found a "MPC5604B_M27V.h" in the problem, but do not know the reason, we can explain to me, specific as follows:

union {
               vuint32_t R;
                  struct {
                                 vuint32_t:7;
                                 vuint32_t NSTART:1;
                                 vuint32_t JABORT:1;
                                 vuint32_t:2;
                                 vuint32_t JSTART:1;
                                  vuint32_t:3;
                                  vuint32_t CTUSTART:1;
                                  vuint32_t CHADDR:7;
                                  vuint32_t:3;
                                  vuint32_t ACK0:1;
 1\\                                 vuint32_t:2;                         // Changed here, and the original is 3
                                  vuint32_t ADCSTATUS:3;
                  } B;
} MSR; /* MAIN STATUS REGISTER */

2\\                           int32_t ADC_reserved2[6];       /* (0x04F - 0x038)/4 = 0x05 */   // The 6 of the brackets were changed to 5

Changed the above two, the ADC interrupt is OK !!!

I would like to ask why!!!!

1 Reply

909 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please share some simple example, which demonstrates your issue?

Regards,

Martin