MPC5604 DSPI  TX/RX FIFO queue bytes size?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5604 DSPI  TX/RX FIFO queue bytes size?

2,910件の閲覧回数
Zhimin
Contributor I

Dear Team:

                   MPC5604 DSPI  TX/RX FIFO queue bytes size?

TKS

 

 

Best Regards,

Atom

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,777件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Which device did you mean?

There is 4-deep TX/RX FIFO on the MPC5604B and 5-deep TX/RX FIFO on the MPC5604P, MPC5604E.

BR, Petr

0 件の賞賛
返信

2,777件の閲覧回数
Zhimin
Contributor I

hi,jive!

can read PC14 input level when config this pin as SPI1 MISO (my target iic is MPC5604B)?

0 件の賞賛
返信

2,777件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

the PC14 cannot be set as SPI1 MISO, did you mean PC4?

For the PC4 if SIU.PCR[36]. IBE bit is set you can read the input level from SIU.GPDI[36] register too.

BR, Petr

0 件の賞賛
返信

2,777件の閲覧回数
Zhimin
Contributor I

TKS!

0 件の賞賛
返信

2,777件の閲覧回数
Zhimin
Contributor I

MPC5604B

0 件の賞賛
返信