MPC5566

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5566

1,920 Views
liuhao11
Contributor I

Dear:

      I have two questions about the 55xx chip.

     What is the detailed difference between mpc5566 and spc5566?  

     From the perspective of hardware and software, can these two chips completely replace each other during use?

    Looking forward to your recovery, thank you very much.

 Respect

0 Kudos
Reply
1 Reply

1,918 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

General rule is as follows:

PPC = Pre-qualification

MPC = Fully spec. qualified, general market flow

SPC = Fully spec. qualified, automotive flow

The same MPC part number may consist of more device masks (revision). SPC part number must be unique, thus it is always the same mask (revision).

I can confirm MPC5566 and SPC5566 are identical parts (if the rest of partnumber is equal) as only one mask exists.

0 Kudos
Reply