MPC555LF4MZP40 versus MPC555LFMZP40

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC555LF4MZP40 versus MPC555LFMZP40

2,922 Views
pjred13
Contributor I

Am i able to use the MPC555LFMZP40 to replace the obsolete MPC555LF4MZP40?

Tags (1)
5 Replies

2,905 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @pjred13 
MPC555LF4MZP40 is old revision K2.
MPC555LFMZP40 is probably latest revision M but it could be also older K3.
The problem is that mask set version is not explicitly mentioned in the part number in case of these old devices.
Older revision Rev K3 stopped shipping WW19/WW20 2005 (WW stands for work week). Only Rev M is shipped after that (talking about general part numbers, not 'SC...' versions).
In case of doubts, the best way is to read IMMR register to check the PARTNUM and MASKNUM. Then you can compare it with this table:

lukaszadrapa_0-1706686615953.png


All these revisions have different errata lists:
https://www.nxp.com/docs/en/errata/MPC555MCE.pdf
https://www.nxp.com/docs/en/errata/MPC555K3CE.pdf
https://www.nxp.com/docs/en/errata/MPC555K2CE.pdf
If you are going to replace one revision with another, it's necessary to compare the errata and re-validate the product.
Newer revisions fix some errata and there are some minor enhancements, so we can't guarantee that it's 100% compatible replacement.

Regards,
Lukas

2,846 Views
fxdurieux
Contributor I

Hi Lukas,

@lukaszadrapa  From what code date can we be sure (at 200% !) that an MPC555LFMZP40 has an M mask (MASKNUM=0x40). Do microcontroller with Freescale marking have only the M mask ? Are all Motorola manufactured devices clearely identified with the mask revision (either by MPC555LF4MZP40 or MPC555LF8MZP40 or maskset number).

Thanks a lot,

Kind regards,
FX D

0 Kudos
Reply

2,823 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @fxdurieux 

attached is product change notification which explicitly talks about MPC555LFMZP40 issued on 9th May 2005. All the devices with this part number manufactured after this date are rev M.

After this date, K3 revision was available only as customer specific part number starting with SC...

Regards,

Lukas

 

0 Kudos
Reply

2,787 Views
fxdurieux
Contributor I

@lukaszadrapa 

Thank you for your answer. Is there a place where i'll be able to find PCN/PDN for MPC555 ? No PDN for this component I hope ...

 

0 Kudos
Reply

2,764 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @fxdurieux

direct customers have an access to our PCN system, distribution customers should get their PCN and PDN from their distributor.
MPC555 Product Discontinuance was issued just two days ago, effective date Feb 13, 2024.
Last time buy date is 12th Aug 2024, last time delivery date is 12th Aug 2025.

Regards,
Lukas

0 Kudos
Reply