MPC5554 software loading using PE Micro Multilink Universal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5554 software loading using PE Micro Multilink Universal

1,036 Views
Vamsi_Tellapandla
Contributor I

I am using Metrowerks IDE with PE Micro Multilink Universal(Part# USB-ML-UNIVERSAL) for code loading with MPC5554 controller. When i am trying to load the code using  64K Starter Edition of P&E's PKGPPCNEXUS it is asking for .asm files and ppf files.As we are using Metrowerks IDE we are having MOT files. Is it possible to load the software using MOT files? Kindly suggest troubleshooting methods for this issue.

 

IMG_20240828_125604.jpgIMG-20240828-WA0003.jpg   

 

 

0 Kudos
Reply
1 Reply

1,013 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

.mot file is S-record, it will ask subsequently
.pcp file a a programming algorithm, it should be present in PKGPPCNEXUS installation directory or it can be downloaded on PeMicro website. Chhose according used board, for instance
Freescale_MPC5554_1x32x512k_Freescale_H7F_32_Driver.PCP

For further detail I would recommend to contact PeMicro support:
https://www.pemicro.com/support/index.cfm

0 Kudos
Reply