MPC5554 software loading using PE Micro Multilink Universal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5554 software loading using PE Micro Multilink Universal

1,050件の閲覧回数
Vamsi_Tellapandla
Contributor I

I am using Metrowerks IDE with PE Micro Multilink Universal(Part# USB-ML-UNIVERSAL) for code loading with MPC5554 controller. When i am trying to load the code using  64K Starter Edition of P&E's PKGPPCNEXUS it is asking for .asm files and ppf files.As we are using Metrowerks IDE we are having MOT files. Is it possible to load the software using MOT files? Kindly suggest troubleshooting methods for this issue.

 

IMG_20240828_125604.jpgIMG-20240828-WA0003.jpg   

 

 

0 件の賞賛
返信
1 返信

1,027件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

.mot file is S-record, it will ask subsequently
.pcp file a a programming algorithm, it should be present in PKGPPCNEXUS installation directory or it can be downloaded on PeMicro website. Chhose according used board, for instance
Freescale_MPC5554_1x32x512k_Freescale_H7F_32_Driver.PCP

For further detail I would recommend to contact PeMicro support:
https://www.pemicro.com/support/index.cfm

0 件の賞賛
返信