MPC5121 FEC DMA TROUBLE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5121 FEC DMA TROUBLE

981 Views
mariosan
Contributor II

Hi, recently I've worken on a board based on a MPC5121 with UBOOT(2013) and running QNX os.

Somethimes after the boot of the OS the FEC do not works at all: resetting it do not works

as expected.  FEC Registers are all OK, but NO TX or RX events are generated, no data are

received or trasmitted. The only event generated is the MII interrupt.

 

UBOOT itself uses the FEC and leave it enabled and fully working before lauch QNX.

Disablig FEC BEFORE launch QNX apparently solves the problem :

I'm figured that problem is in  the descriptors of Tx/Rx ring buffers initialized by UBOOT -

maybe they are somewhat corrupted when OS is loaded in memory, but because FEC

is still active, some incoming ethernet frames will start a DMA in some inappropriate way

and DMA or FEC will goes in some unrecoverable state (You have to RESET the CPU to recovery).

I think that cause the problem but not sure:

Someone found a similar problem?

Can someone explain what the problem is ?

Why FEC isn't working any more also after a ETH_ECNTRL.RESET ?

Is this a MPC5121 undocumented errata?

Thanks

M. Sangalli

 

Labels (1)
0 Kudos
Reply
0 Replies