MCAL software problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCAL software problems

1,442件の閲覧回数
edmundzhang760
Contributor I

1、I encountered the following problems when using MCAL. Please help to confirm the reasons  

The MC_PLLDIG_pClockConfigPB0_0 member in the generated code below has three, but the structure has only two members.  Could you please confirm the reason? Thank you  

The MCAL version is MPC574XP_MCAL_4.0_RTM_HF1_2.0.2  

edmundzhang760_0-1638254447307.jpegedmundzhang760_0-1638254447307.jpegedmundzhang760_1-1638254461562.jpegedmundzhang760_1-1638254461562.jpeg

2、

How many types of MCAL are available for MPC5744?  

The MCAL software package downloaded from the official website provided by your company is not very comprehensive in its functions. May I ask if there are other versions of MCAL, such as the charged version  

タグ(1)
0 件の賞賛
返信
1 返信

1,427件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

As I have checked in Mcu_PLLDIG_Types.h from RTM 2.0.2 HF1, the structure contains three elements:

namnguyenviet_0-1638349128359.pngnamnguyenviet_0-1638349128359.png

 

2. There is RTM 2.0.2 without HF, which you can download in the same place as RTM 2.0.2 HF01. The HF01 contains the fix for MCU driver, which you can find in the Release notes. Other than that, there isn't any MCAL version.

namnguyenviet_1-1638349356788.pngnamnguyenviet_1-1638349356788.png

Best Regards,

Nam

 

0 件の賞賛
返信