Lower FlexRay Bit Rate Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lower FlexRay Bit Rate Support

1,441 Views
cc5447
Contributor I
Dear Sir/Madam,
Hope you are well.
Recently, when I used MFR4310 to debug flexray for communication between two nodes, according to the reference manual, the minimum support is 2.0Mbps. The reference manual needs to change the baud rate field in the mode configuration register and some sampling parameterspdMicrotick,pSamplesPerMicrotick,cSamplesPerBit,cStrobeOffset), but I was confused about the modification of the following parameters. I checked all protocol registers, but no corresponding modification was found. Please also help to see how to modify these parameters?
part of reference manual picture.png
I am looking forward to hearing from you.
Kind regards,
Ms Zhang
Tags (3)
0 Kudos
Reply
0 Replies