Lower FlexRay Bit Rate Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lower FlexRay Bit Rate Support

1,449件の閲覧回数
cc5447
Contributor I
Dear Sir/Madam,
Hope you are well.
Recently, when I used MFR4310 to debug flexray for communication between two nodes, according to the reference manual, the minimum support is 2.0Mbps. The reference manual needs to change the baud rate field in the mode configuration register and some sampling parameterspdMicrotick,pSamplesPerMicrotick,cSamplesPerBit,cStrobeOffset), but I was confused about the modification of the following parameters. I checked all protocol registers, but no corresponding modification was found. Please also help to see how to modify these parameters?
part of reference manual picture.png
I am looking forward to hearing from you.
Kind regards,
Ms Zhang
タグ(3)
0 件の賞賛
返信
0 返答(返信)