LockStep mode and dual parallel mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LockStep mode and dual parallel mode

7,415件の閲覧回数
pramodkashyap
Contributor I

Hello All,

Iam doing a project on EPS(electronic power steering),

Iam looking for a Micro controller with ASIL D complaint,

I looked at this Lockstep mode and dual parallel mode with dual core controllers,

Please can somebody let me know how this two modes will be useful in Hardware/software point of view.

Thanks & Regards,

Pramod Kashyap

0 件の賞賛
返信
2 返答(返信)

6,687件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am attaching several slides describing MPC5643L architecture. It offers two modes LSM and DPM. Page 2 shows their comparison.

Page 3 shows spheres of replication (i.e. Lake) executing the same tasks in LSM mode.

On the place, where replicated and non-replicated part touches, lies redundancy checker. It checks whether bus content is equal - if no, fault is reported to FCCU module and FCCU takes appropriate action (MCU can go to safe mode, interrupt or reset can occur according to particular fault severity, report this condition to supervisory system on FCCU pins and so on).

 

Typical application is in the systems where possible faults are not easily tolerated and malfunction could lead in injuries or damages of people health. It is called safety systems. Examples:

Airbag Systems, Electronic Stability Control, Electric Power Steering, Braking, …

In non-automotive applications Robotics, Industrial Automation, Medical Appliances and so on…

Another point why to use LSM mode for developing your safety application is existence of safety manual what's such guide telling how to develop functional safety system:

http://www.nxp.com/docs/en/user-guide/MPC5643LSM.pdf

You may see following white paper discussing DPM/LSM pros and cons:

http://www.nxp.com/docs/en/white-paper/MPC564XLWP.pdf

To simplify it - LSM is mode is suitable for safety application, DPM for applications where more performance is needed (and integrated special safety HW is disabled).

6,686件の閲覧回数
pramodkashyap
Contributor I

Thanks a lot for response David,

By using the Dual core with lock step mode feature can i reduce the two micro controller architecture in aspect of Hardware as well as software design in functional safety with ASIL D complaint system,

Please can you elaborate more on this doubt.

0 件の賞賛
返信