LinStack availability for MPC5744P?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LinStack availability for MPC5744P?

1,091 Views
Eric_Rabinowitz
Contributor I

Hi, I am using a MCP5744P and building my system with S32 Version 2017.R1.

I want to develop code for the linflexd uart.   I have successfully transmitted raw data using the HAL, but I would prefer to use a full Lin Stack and take advantage of Lin Description Files (ldf) and the flexibility of a stack.

On this board I have seen references to a LinStack for the Kenetis K Family via S32.  Is this library available for the Power Architecture? 

If so, How do I install it in my project?

Thank You

 

0 Kudos
Reply
1 Reply

1,058 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I am forwarding information I have obtained from SDK team:

"Currently there is no plan for the Lin stack to support MPC5744P device.

A solution will be to integrate the latest S32K3 Lin stack that support AUTOSAR LIN driver API with the MPC5744P AUTOSAR MCAL driver package. For this you will need one configuration project S32DS for LIN stack and EB tresos configuration project for AUTOSAR LIN driver. After the generation of the configuration files you should be able to build the Lin stack with the Autosar Lin driver.

The support for SDK driver in the LIN stack is obsolete and will not be supported in future."

0 Kudos
Reply