LINFlexD_LIN module example for MPC5748G is not working ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LINFlexD_LIN module example for MPC5748G is not working ?

1,403 次查看
anishchoudhary
Contributor III

A LINFlexD__LIN module code is  downloaded by me for MPC5748G from S32_Design Studio examples and flash on MPC5748G EVM board and provide 12V on P11.3 pin and try to get data on CRO using P11.4 pin but data is not coming. So i want to know is there any bug in the code or i have to do some other connection on the board ??

标记 (1)
1 回复

1,228 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

example included in S32 Design Studio uses LINFlex0 module which is routed to P9 connector on motherboard. So, connect 12V to P9.3 and measure signal on P9.4.

I tested this and it works correct.

Regards,

Martin