JTAG Connect VLE mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG Connect VLE mode

2,246件の閲覧回数
vincentbergeron
Contributor I

Hi,

 

Im am currently debugging a project using the JTAG connect mode to view disassembly code from a MPC5674F target.  I am using Eclipse CodeWarrior and I want to display VLE instructions in the disassemply window.  How is this possible?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,124件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

is this what you are looking for?

pastedImage_0.png

Regards,

Lukas

0 件の賞賛
返信

2,124件の閲覧回数
vincentbergeron
Contributor I

Not exactly.

I am able to open the disassembly window, but it doesn't recognize the VLE instructions.  Instead, all instructions are on 32 bits and a lot of them are invalid opcodes. 

0 件の賞賛
返信

2,124件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hi

When creating the new project for MPC5674F, please enable the option ‘Use the VLE instruction set’. 

New Project.png

And please also check whether the option ‘Translate PPC Asm to VLE Asm’ and ‘Compress for PowerPC VLE’ are both enabled in project properties.

PowerPC CPU.png

Compiler  Processor.png

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信