Issue with I2C on MPC5606B

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with I2C on MPC5606B

1,418 次查看
malekben
Contributor II

Hi all,

 

I am encountering an issue with my I2C communication :

I am trying to TRANSMIT data in MASTER mode but my program stuck while waiting for IBSR[IBIF] to get set.

This is the code that I am using :

 

//Clear Interrupt Flag

pstIBSRReg = (TstDI2c_iIBSRBits *)(Ctu32DI2c_iBaseAdress[Fu16I2cLink] + Du32DI2c_iIBSROffset);

(* pstIBSRReg).u1IBIF = 1U;

 

//Make sure bus is idle -> IBB must be cleared

while (1U == (* pstIBSRReg).u1IBB) {}

 

//Generate start condition

pstIBCRReg = (TstDI2c_iIBCRBits *)(Ctu32DI2c_iBaseAdress[Fu16I2cLink] + Du32DI2c_iIBCROffset);

(* pstIBCRReg).u1TXRX = 1U; // Transmit

(* pstIBCRReg).u1MSSL = 1U; // Master Mode


//Wait for IBSR.IBB (bus busy) to be set

while (0U == (* pstIBSRReg).u1IBB) {}


//Put target address into IBDR

pstIBDRReg = (TstDI2c_iIBDRBits *)(Ctu32DI2c_iBaseAdress[Fu16I2cLink] + Du32DI2c_iIBDROffset);

(* pstIBDRReg).u8DATA = ((Fu8SlaveID<<1) | Du8DI2c_iWriteSlave);


// Wait for address transfer to be done

while (0U == (* pstIBSRReg).u1IBIF) {}

// Clear Interrupt Flag

(* pstIBSRReg).u1IBIF = 1U;

 

My program stuck at "while (0U == (* pstIBSRReg).u1IBIF) {}".

It is normal because the transfer was not initiated at all since that IBDR register value remains equal to 0x00.

 

Knowing that :

- START signal was correctly generated (verified with a scope).

- After generating the start signal and before writing into IBDR, I2C rgisters value are as below :

* IBCR = 0x30 // MDIS = 0 / MSSL = 1 / TXRX = 1

* IBSR = 0xA0 // TCF = 1 / IBB = 1

- I tried to  write directly on the memory address 0xFFE30004 (IBDR address) but it still always equal to 0x00.

 

My question is what would forbid writing the IBDR register ?

 

 

Best regards,

 

Malek BEN.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,170 次查看
BlackNight
NXP Employee
NXP Employee

Could it be that you run into a silicon errata problem with repeated start condition on I2C?

KL25Z and I2C: Missing Repeated Start Condition | MCU on Eclipse

Erich