Is my STCU2 record correct?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is my STCU2 record correct?

2,853 Views
Furkan_26
Contributor II

Hello,

I am programming the STCU2 module of my MPC5777C mcu. I have used the DCF config generator excel file to write the necessary instructions for offline test both for l and m bists, and I do not have a lot of resources to try for more than 3 times. 

I have generated the following instructions according to the reference manual:

data.set 0x00400310 %QUAD 0xD3FEA98B00080008 ;STCU_SCK 1st write  S30D00400310D3FEA98B000800088A
data.set 0x00400318 %QUAD 0x2C01567400080008  S30D004003182C0156740008000890
data.set 0x00400320 %QUAD 0x0000000000080040 ;STCU_LBU_FM  S30D00400320000000000008004047
data.set 0x00400328 %QUAD 0x0000000000080074 ;STCU_MBU_FML[31:0]  S30D0040032800000000000800740B
data.set 0x00400330 %QUAD 0x0000000000080078 ;STCU_MBU_FMM[31:0]  S30D004003300000000000080078FF
data.set 0x00400338 %QUAD 0x000000000008007C ;STCU_MBU_FMH[31:0]  S30D00400338000000000008007CF3
data.set 0x00400340 %QUAD 0x0000000000080028 ;STCU_ERR_FM  S30D0040034000000000000800283F
data.set 0x00400348 %QUAD 0x0103450400080100 ;STCU_LB_CTRL_0  S30D00400348010345040008010012
data.set 0x00400350 %QUAD 0x000004C000080104 ;STCU_LB_PCS_0  S30D00400350000004C0000801048F
data.set 0x00400358 %QUAD 0x638CABD300080110 ;STCU_LB_MISREL_0  S30D00400358638CABD300080110D2
data.set 0x00400360 %QUAD 0xF6FEF13400080114 ;STCU_LB_MISREH_0  S30D00400360F6FEF134000801141A
data.set 0x00400368 %QUAD 0x0203450400080140 ;STCU_LB_CTRL_1  S30D004003680203450400080140B1
data.set 0x00400370 %QUAD 0x0000034000080144 ;STCU_LB_PCS_1  S30D004003700000034000080144B0
data.set 0x00400378 %QUAD 0x29CAE1DA00080150 ;STCU_LB_MISREL_1  S30D0040037829CAE1DA0008015031
data.set 0x00400380 %QUAD 0xF547396A00080154 ;STCU_LB_MISREH_1  S30D00400380F547396A00080154F4
data.set 0x00400388 %QUAD 0x2C01567400080008 ;STCU_SCK service WDG  S30D004003882C0156740008000820
data.set 0x00400390 %QUAD 0x0303450400080180 ;STCU_LB_CTRL_2  S30D00400390030345040008018048
data.set 0x00400398 %QUAD 0x0000050000080184 ;STCU_LB_PCS_2  S30D00400398000005000008018486
data.set 0x004003A0 %QUAD 0x1AC8F17C00080190 ;STCU_LB_MISREL_2  S30D004003A01AC8F17C0008019028
data.set 0x004003A8 %QUAD 0x84F6497900080194 ;STCU_LB_MISREH_2  S30D004003A884F64979000801942F
data.set 0x004003B0 %QUAD 0x04034504000801C0 ;STCU_LB_CTRL_3  S30D004003B004034504000801C0E7
data.set 0x004003B8 %QUAD 0x00000780000801C4 ;STCU_LB_PCS_3  S30D004003B800000780000801C4A4
data.set 0x004003C0 %QUAD 0x2A96C340000801D0 ;STCU_LB_MISREL_3  S30D004003C02A96C340000801D054
data.set 0x004003C8 %QUAD 0x84756583000801D4 ;STCU_LB_MISREH_3  S30D004003C884756583000801D42A
data.set 0x004003D0 %QUAD 0x0503450400080200 ;STCU_LB_CTRL_4  S30D004003D0050345040008020086
data.set 0x004003D8 %QUAD 0x00000A4000080204 ;STCU_LB_PCS_4  S30D004003D800000A400008020481
data.set 0x004003E0 %QUAD 0x15C9A73F00080210 ;STCU_LB_MISREL_4  S30D004003E015C9A73F00080210F3
data.set 0x004003E8 %QUAD 0xBD55BE6A00080214 ;STCU_LB_MISREH_4  S30D004003E8BD55BE6A0008021471
data.set 0x004003F0 %QUAD 0x7F03450400080240 ;STCU_LB_CTRL_5  S30D004003F07F03450400080240AC
data.set 0x004003F8 %QUAD 0x0000177600080244 ;STCU_LB_PCS_5  S30D004003F80000177600080244DE
data.set 0x00400400 %QUAD 0x9B9F264C00080250 ;STCU_LB_MISREL_5  S30D004004009B9F264C00080250AA
data.set 0x00400408 %QUAD 0x2C01567400080008 ;STCU_SCK service WDG  S30D004004082C015674000800089F
data.set 0x00400410 %QUAD 0xE85AA33F00080254 ;STCU_LB_MISREH_5  S30D00400410E85AA33F000802541E
data.set 0x00400418 %QUAD 0x1100000000080600 ;STCU_MB_CTRL_0  S30D0040041811000000000806007D
data.set 0x00400420 %QUAD 0x1200000000080604 ;STCU_MB_CTRL_1  S30D00400420120000000008060470
data.set 0x00400428 %QUAD 0x1300000000080608 ;STCU_MB_CTRL_2  S30D00400428130000000008060863
data.set 0x00400430 %QUAD 0x140000000008060C ;STCU_MB_CTRL_3  S30D00400430140000000008060C56
data.set 0x00400438 %QUAD 0x1500000000080610 ;STCU_MB_CTRL_4  S30D00400438150000000008061049
data.set 0x00400440 %QUAD 0x1600000000080614 ;STCU_MB_CTRL_5  S30D0040044016000000000806143C
data.set 0x00400448 %QUAD 0x1700000000080618 ;STCU_MB_CTRL_6  S30D0040044817000000000806182F
data.set 0x00400450 %QUAD 0x180000000008061C ;STCU_MB_CTRL_7  S30D00400450180000000008061C22
data.set 0x00400458 %QUAD 0x1900000000080620 ;STCU_MB_CTRL_8  S30D00400458190000000008062015
data.set 0x00400460 %QUAD 0x1A00000000080624 ;STCU_MB_CTRL_9  S30D004004601A0000000008062408
data.set 0x00400468 %QUAD 0x1B00000000080628 ;STCU_MB_CTRL_10  S30D004004681B00000000080628FB
data.set 0x00400470 %QUAD 0x1C0000000008062C ;STCU_MB_CTRL_11  S30D004004701C0000000008062CEE
data.set 0x00400478 %QUAD 0x1D00000000080630 ;STCU_MB_CTRL_12  S30D004004781D00000000080630E1
data.set 0x00400480 %QUAD 0x2C01567400080008 ;STCU_SCK service WDG  S30D004004802C0156740008000827
data.set 0x00400488 %QUAD 0x1E00000000080634 ;STCU_MB_CTRL_13  S30D004004881E00000000080634CC
data.set 0x00400490 %QUAD 0x1F00000000080638 ;STCU_MB_CTRL_14  S30D004004901F00000000080638BF
data.set 0x00400498 %QUAD 0x200000000008063C ;STCU_MB_CTRL_15  S30D00400498200000000008063CB2
data.set 0x004004A0 %QUAD 0x2100000000080640 ;STCU_MB_CTRL_16  S30D004004A02100000000080640A5
data.set 0x004004A8 %QUAD 0x2200000000080644 ;STCU_MB_CTRL_17  S30D004004A8220000000008064498
data.set 0x004004B0 %QUAD 0x2300000000080648 ;STCU_MB_CTRL_18  S30D004004B023000000000806488B
data.set 0x004004B8 %QUAD 0x240000000008064C ;STCU_MB_CTRL_19  S30D004004B8240000000008064C7E
data.set 0x004004C0 %QUAD 0x2500000000080650 ;STCU_MB_CTRL_20  S30D004004C0250000000008065071
data.set 0x004004C8 %QUAD 0x2600000000080654 ;STCU_MB_CTRL_21  S30D004004C8260000000008065464
data.set 0x004004D0 %QUAD 0x2700000000080658 ;STCU_MB_CTRL_22  S30D004004D0270000000008065857
data.set 0x004004D8 %QUAD 0x280000000008065C ;STCU_MB_CTRL_23  S30D004004D8280000000008065C4A
data.set 0x004004E0 %QUAD 0x2900000000080660 ;STCU_MB_CTRL_24  S30D004004E029000000000806603D
data.set 0x004004E8 %QUAD 0x2A00000000080664 ;STCU_MB_CTRL_25  S30D004004E82A0000000008066430
data.set 0x004004F0 %QUAD 0x2B00000000080668 ;STCU_MB_CTRL_26  S30D004004F02B0000000008066823
data.set 0x004004F8 %QUAD 0x2C0000000008066C ;STCU_MB_CTRL_27  S30D004004F82C0000000008066C16
data.set 0x00400500 %QUAD 0x2D00000000080670 ;STCU_MB_CTRL_28  S30D004005002D0000000008067008
data.set 0x00400508 %QUAD 0x2E00000000080674 ;STCU_MB_CTRL_29  S30D004005082E00000000080674FB
data.set 0x00400510 %QUAD 0x2C01567400080008 ;STCU_SCK service WDG  S30D004005102C0156740008000896
data.set 0x00400518 %QUAD 0x2F00000000080678 ;STCU_MB_CTRL_30  S30D004005182F00000000080678E6
data.set 0x00400520 %QUAD 0x300000000008067C ;STCU_MB_CTRL_31  S30D00400520300000000008067CD9
data.set 0x00400528 %QUAD 0x3100000000080680 ;STCU_MB_CTRL_32  S30D004005283100000000080680CC
data.set 0x00400530 %QUAD 0x3200000000080684 ;STCU_MB_CTRL_33  S30D004005303200000000080684BF
data.set 0x00400538 %QUAD 0x3300000000080688 ;STCU_MB_CTRL_34  S30D004005383300000000080688B2
data.set 0x00400540 %QUAD 0x340000000008068C ;STCU_MB_CTRL_35  S30D00400540340000000008068CA5
data.set 0x00400548 %QUAD 0x3500000000080690 ;STCU_MB_CTRL_36  S30D00400548350000000008069098
data.set 0x00400550 %QUAD 0x3600000000080694 ;STCU_MB_CTRL_37  S30D0040055036000000000806948B
data.set 0x00400558 %QUAD 0x3700000000080698 ;STCU_MB_CTRL_38  S30D0040055837000000000806987E
data.set 0x00400560 %QUAD 0x380000000008069C ;STCU_MB_CTRL_39  S30D00400560380000000008069C71
data.set 0x00400568 %QUAD 0x39000000000806A0 ;STCU_MB_CTRL_40  S30D0040056839000000000806A064
data.set 0x00400570 %QUAD 0x3A000000000806A4 ;STCU_MB_CTRL_41  S30D004005703A000000000806A457
data.set 0x00400578 %QUAD 0x3B000000000806A8 ;STCU_MB_CTRL_42  S30D004005783B000000000806A84A
data.set 0x00400580 %QUAD 0x3C000000000806AC ;STCU_MB_CTRL_43  S30D004005803C000000000806AC3D
data.set 0x00400588 %QUAD 0x3D000000000806B0 ;STCU_MB_CTRL_44  S30D004005883D000000000806B030
data.set 0x00400590 %QUAD 0x3E000000000806B4 ;STCU_MB_CTRL_45  S30D004005903E000000000806B423
data.set 0x00400598 %QUAD 0x3F000000000806B8 ;STCU_MB_CTRL_46  S30D004005983F000000000806B816
data.set 0x004005A0 %QUAD 0x2C01567400080008 ;STCU_SCK service WDG  S30D004005A02C0156740008000806
data.set 0x004005A8 %QUAD 0x40000000000806BC ;STCU_MB_CTRL_47  S30D004005A840000000000806BC01
data.set 0x004005B0 %QUAD 0x41000000000806C0 ;STCU_MB_CTRL_48  S30D004005B041000000000806C0F4
data.set 0x004005B8 %QUAD 0x42000000000806C4 ;STCU_MB_CTRL_49  S30D004005B842000000000806C4E7
data.set 0x004005C0 %QUAD 0x43000000000806C8 ;STCU_MB_CTRL_50  S30D004005C043000000000806C8DA
data.set 0x004005C8 %QUAD 0x44000000000806CC ;STCU_MB_CTRL_51  S30D004005C844000000000806CCCD
data.set 0x004005D0 %QUAD 0x45000000000806D0 ;STCU_MB_CTRL_52  S30D004005D045000000000806D0C0
data.set 0x004005D8 %QUAD 0x46000000000806D4 ;STCU_MB_CTRL_53  S30D004005D846000000000806D4B3
data.set 0x004005E0 %QUAD 0x47000000000806D8 ;STCU_MB_CTRL_54  S30D004005E047000000000806D8A6
data.set 0x004005E8 %QUAD 0x48000000000806DC ;STCU_MB_CTRL_55  S30D004005E848000000000806DC99
data.set 0x004005F0 %QUAD 0x49000000000806E0 ;STCU_MB_CTRL_56  S30D004005F049000000000806E08C
data.set 0x004005F8 %QUAD 0x4A000000000806E4 ;STCU_MB_CTRL_57  S30D004005F84A000000000806E47F
data.set 0x00400600 %QUAD 0x4B000000000806E8 ;STCU_MB_CTRL_58  S30D004006004B000000000806E871
data.set 0x00400608 %QUAD 0x4C000000000806EC ;STCU_MB_CTRL_59  S30D004006084C000000000806EC64
data.set 0x00400610 %QUAD 0x4D000000000806F0 ;STCU_MB_CTRL_60  S30D004006104D000000000806F057
data.set 0x00400618 %QUAD 0x4E000000000806F4 ;STCU_MB_CTRL_61  S30D004006184E000000000806F44A
data.set 0x00400620 %QUAD 0x4F000000000806F8 ;STCU_MB_CTRL_62  S30D004006204F000000000806F83D
data.set 0x00400628 %QUAD 0x50000000000806FC ;STCU_MB_CTRL_63  S30D0040062850000000000806FC30
data.set 0x00400630 %QUAD 0x0000000000080700 ;STCU_MB_CTRL_64  S30D00400630000000000008070074
data.set 0x00400638 %QUAD 0xFFFFFFFF00080014 ;STCU_WDG  S30D00400638FFFFFFFF000800145C
data.set 0x00400640 %QUAD 0x1000000D0008000C ;STCU_CFG  S30D004006401000000D0008000C3B
data.set 0x00400648 %QUAD 0x0205003200080010 ;STCU_PLL_CFG  S30D00400648020500320008001013
data.set 0x00400650 %QUAD 0x0000030100080000 ;STCU_RUN  S30D00400650000003010008000050

 

I must add that this excel file generates wrong checksum values for some srec records, and I use them via a script I have wrote by using Python. 

Could you verify if my instructions are correct or not? If I embed the corrected srec to the mcu, is it going to work? Can I show if STCU2 module is working correctly via a manual or a paper? Because as far as I understand, there is no way to corrupt the device without actually harming it. 

Thanks in advance.

Best wishes 

0 Kudos
Reply
5 Replies

2,828 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Well, programming the STCU based on your own configuration.. I would not recommend doing that unless you have deep knowledge on STCU mechanism and lot of testing possibility.

Could you verify if my instructions are correct or not?

I have attached reference script. Furthermore checksums depends on device cut, which you do not share with me. So make sure you have the same as I. -> 3N45H

If I embed the corrected srec to the mcu, is it going to work?

Cant say. But if it is correct STCU configuration validated by NXP, it will.

Can I show if STCU2 module is working correctly via a manual or a paper?

Sorry, I do not understand this questions. STCU is HW module operating dependent on voltages, memory conditions, peripheries, etc...

Because as far as I understand, there is no way to corrupt the device without actually harming it.

By programming STCU DCF records, you cant harm device. But messing with UTEST flash, you definitely can corrupt device.

I suggest you to read AN:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC57xx-DCF-records/ta-p/1114884

 

https://www.nxp.com/docs/en/application-note/AN5288.pdf

 

 

Best regards,

Peter

0 Kudos
Reply

2,823 Views
Furkan_26
Contributor II

@petervlna Thank you for explaining.

Sorry, I do not understand this questions. STCU is HW module operating dependent on voltages, memory conditions, peripheries, etc...

I must validate my configuration work somehow for certification. So ı need some result of testing by you. 

how can I run the cmm file? Im using PE micro FX debugger is that important for implementing that script?

I have attached reference script. Furthermore checksums depends on device cut, which you do not share with me. So make sure you have the same as I. -> 3N45H

I meant the checksums the excel calculates.

0 Kudos
Reply

2,807 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I must validate my configuration work somehow for certification. So ı need some result of testing by you.

Dont know which kind of certification standard you are talking about. This device is ASIL-D ready.

Anyway, we are not able to share any resources regarding testing process here on public community.

For such communication you will need NDA and rise a ticket at NXP.com

how can I run the cmm file? Im using PE micro FX debugger is that important for implementing that script?

You will need Lauterbach debugger in order to use cmm file.

I have shared it as an example of configuration. You can port the DCFs for your PE which use S3 records format.

I meant the checksums the excel calculates.

Excel should be fine. But I was talking about BIST MISR checksums. Those are MISR trough registers and they differ based on silicon cut. So make sure you have same device cut.

Otherwise when the BIST finish logic tests, it will fail as the expected and calculated MISR will not match.

Unfortunate I do not have PE script for BIST programming. Not even sure if PE allows scripting.

Best regards,

Peter

2,800 Views
marv_marsian
Contributor II

Hey @petervlna and @Furkan_26,

I also had a similar problem about the excel. 

So make sure you have same device cut.

How to check this? What is a device cut? 

 

0 Kudos
Reply

2,782 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

You can read MIDR register.

Or simply have a look at device package:

petervlna_0-1668154894830.png

 

Best regards,

Peter