Interrupt Vector Number in MPC5777M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interrupt Vector Number in MPC5777M

2,964件の閲覧回数
yalamandadosaky
Contributor V

Hi PetrS martinkovar, Is there anyway that I can read IRQ (through register) numbers during run time for CAN node in MPC5777M .

suppose for M_CAN_1 the IRQ are 688 and 689.

So I want to read these numbers run time and raise the particular ISR.

タグ(1)
4 返答(返信)

2,517件の閲覧回数
yalamandadosaky
Contributor V

Any Update?

0 件の賞賛
返信

2,517件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am afraid your question does not make too much sense to us. Could you please ask different way letting us to understand your question? Thanks

2,517件の閲覧回数
yalamandadosaky
Contributor V

Thank you , OK . My requirement is like single ISR function to be used in my function and I want to call this function by checking IRQ number so that I can pass the parameters corresponding to that IRQ number.

Example :

ISR(x)

{

/// code

}

if(IRQ == 688u)

{

ISR(M_CAN_1)

}

else if (IRQ == 689u)

{

ISR(M_CAN2)

}

So through which register I can read IRQ number that caused the interrupt during runtime ?

0 件の賞賛
返信

2,517件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

the solution you try to create is definitely not correct way, how interrupts should work or be implemented. 

Correct way is to implement interrupt using peripheral interrupt registers and INTC controller configuration. Another way is to use polling, it means check peripheral interrupt flag by software.

Please look at the following example. It shows, how to use FlexCAN with interrupts. Example is not created for MPC5777M and MCAN module, but for MPC5775K and FlexCAN module, but the idea of using interrupts is the same.

Example MPC5775K FlexCAN_with_interrupts_v1.1 S32DS 

For correct polling method implementation, please see the example below:

Example MPC5777M MCAN simple TX/RX GHS614 

Please do not try to use the way you designed. It can cause unpredictable microcontroller behavior. 

Regards,

Martin