Internal Pullup Issue in MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Internal Pullup Issue in MPC5744P

Jump to solution
1,568 Views
hityouxinxin
Contributor II

Hello:

   There is a question when I use MPC5744P,I want to use internal pullup on PB[13],but I failed.

   When I try to set PUE and PUS bit in MSCR register,it always 0.In RM,I found this table,the NA means PB[13] could not using internal PUS?

pastedImage_2.png

pastedImage_1.png

Tags (1)
0 Kudos
Reply
1 Solution
1,513 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

yes, that is correct. On B[13] there is no pulup available as table 4-16 describes.

As you can see it is connected to ADC1_AN[0] channel by default.

pastedImage_1.png

regards,

Peter

View solution in original post

1 Reply
1,514 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

yes, that is correct. On B[13] there is no pulup available as table 4-16 describes.

As you can see it is connected to ADC1_AN[0] channel by default.

pastedImage_1.png

regards,

Peter