Importing NXP Example Projects into CodeWarrior for MCU v10.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Importing NXP Example Projects into CodeWarrior for MCU v10.6

1,398件の閲覧回数
mertk
Contributor IV

Hi everyone,

I am a newbie and I have struggled to import NXP examples into the CodeWarrior for MCU v10.6. 

For instance for NXP Example Project;

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5674F-1b-2b-RAM-ECC-error-injection-C...

I couldn't achieve to import this project into the CodeWarrior for MCU v10.6. When I want to import all .c and .h files and build the project, there are lots of errors. 

Therefore, can you give me a hand?

Best regards,

Mert.

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,384件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

there is no direct import option, I guess, so a recommendation could be to create new project in CW10.6 and copy relevant portion of code from main.c uart.c files (. Do it per short piece of code and build between, so can easily fix possible errors.

BR, Petr

0 件の賞賛
返信

1,376件の閲覧回数
mertk
Contributor IV

Hi @PetrS 

Thanks for your answer. I will try to import step by step. But I am wondering why NXP Project Example folder structures are different CW for MCU? Is it an old structure or a new structure with respect to CW for MCU 10.6? 

Best Regards,

Mert. 

0 件の賞賛
返信