Importing NXP Example Projects into CodeWarrior for MCU v10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Importing NXP Example Projects into CodeWarrior for MCU v10.6

1,387 Views
mertk
Contributor IV

Hi everyone,

I am a newbie and I have struggled to import NXP examples into the CodeWarrior for MCU v10.6. 

For instance for NXP Example Project;

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5674F-1b-2b-RAM-ECC-error-injection-C...

I couldn't achieve to import this project into the CodeWarrior for MCU v10.6. When I want to import all .c and .h files and build the project, there are lots of errors. 

Therefore, can you give me a hand?

Best regards,

Mert.

Tags (1)
0 Kudos
Reply
2 Replies

1,373 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

there is no direct import option, I guess, so a recommendation could be to create new project in CW10.6 and copy relevant portion of code from main.c uart.c files (. Do it per short piece of code and build between, so can easily fix possible errors.

BR, Petr

0 Kudos
Reply

1,365 Views
mertk
Contributor IV

Hi @PetrS 

Thanks for your answer. I will try to import step by step. But I am wondering why NXP Project Example folder structures are different CW for MCU? Is it an old structure or a new structure with respect to CW for MCU 10.6? 

Best Regards,

Mert. 

0 Kudos
Reply