Imported example error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imported example error

2,396 Views
asua
Contributor I

I import the example 'MPC5746R_PinToggleStationery_S32DS_Power_2017.R1', 

but when I 'build the project', it prompt some error,  also 2 warinings.

The detail info of errors are:

Errors occurred during the build.
Errors running builder 'CDT Builder' on project 'MPC5746R_PinToggleStationery_S32DS_Z4_1'.
Resource '/MPC5746R_PinToggleStationery_S32DS_Z4_1/Debug/sources.mk' does not exist.
Resource '/MPC5746R_PinToggleStationery_S32DS_Z4_1/Debug/sources.mk' does not exist.

Thanks very much,

asua

 

 

 

 

0 Kudos
Reply
5 Replies

2,386 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Which version of S32DS for power have you used?

Best regards,

Peter

0 Kudos
Reply

2,384 Views
asua
Contributor I

asua_0-1673481684415.png

 

0 Kudos
Reply

2,380 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Then the issue is that you are running 'MPC5746R_PinToggleStationery_S32DS_Power_2017.R1

SW on the S32DS v2.1 which is not compatible.

Please use the embedded examples in S32DS v2.1 instead.

petervlna_0-1673511946393.png

Best regards,

Peter

 

0 Kudos
Reply

2,373 Views
asua
Contributor I

Hi, Peter

So what does the RTM mean in the directory 'SDK PA RTM v3.0.0 Example Projects'?

What is the difference between the examples in this directory  and  in the directory of ' S32DS Example Projects'?

Thank you very much

Best Regards,

asua

0 Kudos
Reply

2,367 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

So what does the RTM mean in the directory 'SDK PA RTM v3.0.0 Example Projects'?

RTM - release to market

What is the difference between the examples in this directory and in the directory of ' S32DS Example Projects'?

different drivers types. SDK and bare metal.

Best regards,

Peter

0 Kudos
Reply