IBIS model for MPC5534 Microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IBIS model for MPC5534 Microcontroller

6,727 Views
nileshkhupase
Contributor I

Dear sir or Madam,

 

Is there an IBIS model for MPC5534 Microcontroller?

 

Many Thanks in advance.

Labels (1)
0 Kudos
Reply
5 Replies

5,331 Views
Shweta_chendake
Contributor I

 can we use IBIS model of MPC5554 instead of MPC5534?

and if yes then please send the  associated pin numbers in the MPC5554 model that have the same function as those in the MPC5534 model.

  • SCKC( K20)-
  • SINC( J20) -
  • SOUTC (K22) -
  • PCSC3 (AB18) -
  • SCKD (M21) -
  • SIND (K19) -
  • SOUTD (N19)-
  • PCSD0 (J22) -

 

Ans if No, can you please send the generic IBIS model for MPC5534?

0 Kudos
Reply

6,592 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Unfortunately we don't have a specific ibis model for the MPC5534.

We have a general ibis model for the MPC555x/MPC556x family of products, on the link below:

http://www.nxp.com/webapp/sps/download/license.jsp?colCode=MPC5554_IBIS&location=null&Parent_nodeId=...

The name of the file states MPC5554, however, it applies to all MPC555x/MPC556x family devices.

0 Kudos
Reply

6,591 Views
nileshkhupase
Contributor I

Dear Sir or Madam,

Thank you very much for your reply. Can I refer the same IBIS model for MPC5534 device? Does MPC5534 belong to MPC555x/MPC556x family?

Best regards,

Nilesh Khupase

0 Kudos
Reply

6,591 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

To be more precise it is MPC5500 family and devices are somehow compatible to each other:

http://cache.nxp.com/files/32bit/doc/eng_bulletin/EB659.pdf

0 Kudos
Reply

6,590 Views
nileshkhupase
Contributor I

Hi David,

That means we do not have IBIS model for MPC5500 family. Can we use the available IBIS model (MPC5554)?

Thanks,

Nilesh

0 Kudos
Reply