How to use DMA Scatter/Gather?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use DMA Scatter/Gather?

ソリューションへジャンプ
4,711件の閲覧回数
liujinhang
Contributor III

Dear All,

            I want to use  DMA Scatter/Gather function of MPC5444P,but some experiment phenomenon Confused me,the following is my DMA configurations information:

      177821_177821.png123.png

177822_177822.png321.png

Problem phenomenon:when the major loop completed,the value of DMA_0.TCD[18].DLASTSGA.B.DLASTSGA was added to the DMA_0.TCD[18].DADDR.B.DADDR rather than  the contents of TCD_SG1[]  is loaded into the TCD register, then a DMA Destination Bus Error occurred.

 Can anyone tell me how can i do to make the contents of TCD_SG1[] be loaded into the TCD register ?

here is the reference:http://cache.nxp.com/assets/documents/data/en/application-notes/AN4765.pdf?fromsite=zh-Hans 

thanks very much!

ラベル(1)
1 解決策
4,181件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Do you have you scatter/gather descriptor 32bytes aligned in memory?

This is mandatory.

Peter

元の投稿で解決策を見る

5 返答(返信)
4,181件の閲覧回数
enes
Contributor II

Hi, we have same problem with scatter-gather method. Can u give more details about how to solve this problem. 

0 件の賞賛
返信
4,181件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Just align your TCD in memory for 32bytes. Otherwise DMA will load incomplete or incorrect TCD.

PEter

4,182件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Do you have you scatter/gather descriptor 32bytes aligned in memory?

This is mandatory.

Peter

4,181件の閲覧回数
liujinhang
Contributor III

It maybe the problem,The addresses of TCD_SG0[] and TCD_SG1[] are really not 32bytes aligned in memory . I misunderstood  the meaning of "0-modulo-32-byte",  thank you for your reminding!

but I do not know how to make the scatter/gather descriptor 32bytes aligned  in memory. Can you give me an example?

 thanks very much!

0 件の賞賛
返信
4,181件の閲覧回数
liujinhang
Contributor III

hi, Peter 

I did it ,thanks for your reply.

Best Wishes

0 件の賞賛
返信