How to solve speed ambiguity of automotive radar ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to solve speed ambiguity of automotive radar ?

ソリューションへジャンプ
2,907件の閲覧回数
pingfang
Contributor III

Hello,

How to solve speed ambiguity  of automotive radar ? Can you give me some suggestions?

Thank you.

0 件の賞賛
返信
1 解決策
2,711件の閲覧回数
ewanharwood
NXP Employee
NXP Employee

Hi pingfang,

The Doppler Ambiguity can be solved in different ways and will be dependent on the radar system under development, this is the task of the customer to define the radar system.

 

In order to avoid Doppler ambiguities, radar systems require high pulse repetition frequency (PRF) rates when detecting high-speed targets. When a long-range radar is required to detect a high-speed target, it may not be possible to be both range and Doppler unambiguous. This problem can be resolved by using multiple PRFs. Multiple PRF schemes can be incorporated sequentially within each dwell interval (scan or integration frame) or the radar can use a single PRF in one scan and resolve ambiguity in the next. The latter technique, however, may have problems due to changing target dynamics from one scan to the next. The Doppler ambiguity problem is analogous to that of range ambiguity. Therefore, the same methodology can be used to resolve Doppler ambiguity.

Hopefully this helps direct your research.

Thanks,

Ewan 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,712件の閲覧回数
ewanharwood
NXP Employee
NXP Employee

Hi pingfang,

The Doppler Ambiguity can be solved in different ways and will be dependent on the radar system under development, this is the task of the customer to define the radar system.

 

In order to avoid Doppler ambiguities, radar systems require high pulse repetition frequency (PRF) rates when detecting high-speed targets. When a long-range radar is required to detect a high-speed target, it may not be possible to be both range and Doppler unambiguous. This problem can be resolved by using multiple PRFs. Multiple PRF schemes can be incorporated sequentially within each dwell interval (scan or integration frame) or the radar can use a single PRF in one scan and resolve ambiguity in the next. The latter technique, however, may have problems due to changing target dynamics from one scan to the next. The Doppler ambiguity problem is analogous to that of range ambiguity. Therefore, the same methodology can be used to resolve Doppler ambiguity.

Hopefully this helps direct your research.

Thanks,

Ewan 

0 件の賞賛
返信