How to setup eMIOS QDEC function?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to setup eMIOS QDEC function?

ソリューションへジャンプ
5,538件の閲覧回数
daniel_fernande
Contributor III

Hi, 

I would like to test the QDEC function of the eMIOS. I am working with MPC5777C on the evaluation board.

I am generating A/B 1khz 90° shift square signals on the EMIOS0/1 channels and I have configured the eMIOS this way : 

// IO Pin configuration

emios_configInpuQD = PA_PRIF | IBE;
//eMIOS 0 channel 0
SIU.PCR[179].R = emios_configInpuQD;
//eMIOS 0 channel 1
SIU.PCR[180].R = emios_configInpuQD;

//eMIOS configuration

eMIOS_0.MCR.B.GPRE= 63; /* Divide 64 MHz sysclk by 63+1 = 64 for 1MHz eMIOS clk*/
eMIOS_0.MCR.B.ETB = 1; /* External time base is disabled; Ch 23 drives ctr bus A */
eMIOS_0.MCR.B.FRZ = 1; /* Enable stopping channels when in debug mode */

eMIOS_0.UC[0].C.B.BSL = 3; // Use internal counters?
eMIOS_0.UC[1].C.B.BSL = 3; // Use internal counters
eMIOS_0.UC[1].C.B.MODE = 0x0D; /* Quadrature decode (for phase A and phase B encoders type) */

eMIOS_0.MCR.B.GPREN = 1; /* Enable eMIOS clock */
eMIOS_0.MCR.B.GTBE = 1; /* Enable global time base */

I am expecting the see the CNT register of UC(1) incrementing but nothing is happening, looks like I'm missing something very basic. Any clue?

Many thanks, 

Daniel

タグ(2)
1 解決策
5,269件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you will need to configure IGF module, otherwise inputs does not pass to eMIOS module.

IGF_0.FILTER[16].MCR.B.FGEN = 1;

IGF_0.FILTER[17].MCR.B.FGEN = 1;

BR, Petr

元の投稿で解決策を見る

4 返答(返信)
5,269件の閲覧回数
阮浩ruanhaosk
Contributor I

Hi, 

 

I would like to test the QDEC function of the eMIOS. I am working with MPC5634 on the evaluation board.

I am generating A/B 1khz 90° shift square signals on the EMIOS8/9 channels and I have configured the eMIOS this way

//MPC5634 - EMIOS -QDEC 

void vfn_emios_Qdec_set(uint8_t ui8_chan)
{
EMIOS.CH[ui8_chan-1].CCR.B.MODE= 0x00;
EMIOS.CH[ui8_chan-1].CCNTR.R = 10000;
EMIOS.CH[ui8_chan-1].CADR.R = 10000;
EMIOS.CH[ui8_chan-1].CBDR.R = 10000;
EMIOS.CH[ui8_chan-1].CCR.B.BSL = 0;
EMIOS.CH[ui8_chan-1].CCR.B.UCPRE = 0;
EMIOS.CH[ui8_chan-1].CCR.B.UCPREN = 1;
EMIOS.CH[ui8_chan-1].CCR.B.EDPOL = 1;

EMIOS.CH[ui8_chan-1].CCR.B.IF= 0x08;
EMIOS.CH[ui8_chan-1].CCR.B.EDSEL=0;
EMIOS.CH[ui8_chan-1].CCR.B.DMA=0;
EMIOS.CH[ui8_chan-1].CCR.B.FEN = 1;

EMIOS.CH[ui8_chan-1].CCR.B.MODE= 0x10;
// EMIOS.CH[ui8_chan-1].CCR.B.MODE= 0x4;

EMIOS.CH[ui8_chan-1].CADR.R = 1;
SIU.PCR[187].R = 0x0500; /* Initialize pad for eMIOS chan. 2 output */

EMIOS.CH[ui8_chan].CCR.B.MODE= 0x00;
EMIOS.CH[ui8_chan].CCNTR.R = 10000;
EMIOS.CH[ui8_chan].CADR.R = 10000;
EMIOS.CH[ui8_chan].CBDR.R = 10000;
EMIOS.CH[ui8_chan].CCR.B.BSL = 0;
EMIOS.CH[ui8_chan].CCR.B.UCPRE = 0;
EMIOS.CH[ui8_chan].CCR.B.UCPREN = 1;
EMIOS.CH[ui8_chan].CCR.B.EDPOL = 1;
;
EMIOS.CH[ui8_chan].CCR.B.IF= 0x08;
EMIOS.CH[ui8_chan].CCR.B.EDSEL=0;
EMIOS.CH[ui8_chan].CCR.B.DMA=0;
EMIOS.CH[ui8_chan].CCR.B.FEN = 1;

EMIOS.CH[ui8_chan].CCR.B.MODE= 0x0D;
// EMIOS.CH[ui8_chan].CCR.B.MODE= 0x02;

EMIOS.CH[ui8_chan].CADR.R = 1;
SIU.PCR[188].R = 0x0500; /*4 Initialize pad for eMIOS chan. 2 output */
}

Many thanks, 

RH

0 件の賞賛
返信
5,269件の閲覧回数
daniel_fernande
Contributor III

Thanks that was the problem !

Maybe additional question : 

Ok now Im trying to drive global counter A with the encoder events. 

So I'm configuring UC[23] in QDEC mode and this channel is working fine, I can see the internal counter of UC[23] incrementing correctly but I am not sure if counter A is incrementing

Now I want to configure for example UC[20] with a modulo 4096 driven by counter A, but unfortunatelly this does not work. 

Here is my configuration : 

pastedImage_1.png

Regards, 

Daniel

0 件の賞賛
返信
5,269件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

unfortunately counter wrap (e.g. 4095->0 when counting up, 0>4095 when counting down) is not supported by HW for QDEC mode. Neither I do not see SW workaround. You can set CADR register to generate flag on counter match, but this does not bring big benefit.

When ch 23 is running in QDEC mode, its internal counter is providing counter bus A. 

If using MC, MCB modes the internal counter is always selected.

BR, Petr

0 件の賞賛
返信
5,269件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you will need to configure IGF module, otherwise inputs does not pass to eMIOS module.

IGF_0.FILTER[16].MCR.B.FGEN = 1;

IGF_0.FILTER[17].MCR.B.FGEN = 1;

BR, Petr