How to configure  CAN of  MPC5605B to receive a remote frame?  

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure  CAN of  MPC5605B to receive a remote frame?  

1,312 Views
spring236869
Contributor I

now I have configure the CAN of 5605B,  it can transmit a remote frame ,  but it can not  receive  a  remote frame.

How configure it?

could you  give a example project to me?

Labels (1)
0 Kudos
Reply
1 Reply

1,218 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

This is clearly described in FlexCAN's chapter “Remote Frames” of the RM.

  

FlexCAN can receive Remote Frame, but does not store it into a regular message buffer. You can configure TX MB to do a response to the received Remote Frame. When a Remote Request frame is received by FlexCAN, its ID is compared to the IDs of the transmit message buffers with the Code field ‘1010’. If there is a matching ID, then this MB frame will be transmitted.

If the RX FIFO is enabled the received Remote Frame can be stored into FIFO. In this case FlexCAN will not generate an automatic response for Remote Request Frames that match the FIFO filtering criteria. If the Remote Frame matches one of the target IDs, it will be stored in the FIFO and presented to the CPU.

BR, Petr

0 Kudos
Reply