How to Enter Debug Mode on MPC5748G ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to Enter Debug Mode on MPC5748G ?

跳至解决方案
8,038 次查看
kimyoungsu
Contributor III

173861_173861.pngt32_diff.png

 

MPC5646C is entered debug mode but MPC5748G is not entered debug mode.

 

ssd c55 flash driver load to sram and  set PC and go.

but it is not go.

 

plz help how to go+exit ?

Original Attachment has been moved to: JTAG_MPC5646C.cmm.zip

Original Attachment has been moved to: JTAG_MPC5748G.cmm.zip

标签 (1)
1 解答
7,313 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there's se_illegal instruction (0x0000) between two nop instructions (ori r0,r0,0x0). If this instruction is executed in external debug mode then debug mode is entered.

pastedImage_1.png

I tested it and it works as expected. It is necessary to set BDMEnabled to TRUE and then this code is executed at the end of function.

My question is: how did you set r1, r3 and ssd_config structure before executing the function?

Regards,

Lukas

在原帖中查看解决方案

0 项奖励
回复
10 回复数
7,312 次查看
ferencvalenta
Contributor III

Hi,

The original cmm worked for me with old versions of the Calypso (1N81M), but it does not with the latest version (0N78S). Same symptom, debug mode not entered. Note the different JTAG ID for the new MCU.

Any ideas how to enter debug mode on this device?

JTAG demo
--------------------------------------------------------
  JTAGC reset
  ------------------------------------------------------
  Reading JTAG_IDCODE
  IDCODE=0x0988201D
  ------------------------------------------------------
  Enabling OnCE
  ------------------------------------------------------
  Enter debug mode during reset:
  Asserting RESET
  Writing OCR - set OCR[DR] and set OCR[WKUP]
  Deasserting RESET
  Verify status register
  STATUS=0x00000201
  ------------------------------------------------------
  Disable watchdog
    Data=0x0A0100FF
  ------------------------------------------------------
  Verify status register
  STATUS=0x00000201

0 项奖励
回复
7,312 次查看
ferencvalenta
Contributor III

Oops it works, but somehow slower than Cut 2.0. The 100ms delay is really needed. 1N81M worked with 50us.

0 项奖励
回复
7,313 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I could see that the device was reset by watchdog, so I modified the script to disable the watchdog after reset deassertion. Then it works fine on my side:

pastedImage_1.png

Regards,

Lukas

7,313 次查看
kimyoungsu
Contributor III

FlashInit VLE Assem code under

Where is BDM Enable code on C55 SRecord Firmware VLE Assem?

c55_flashinit.png

0 项奖励
回复
7,314 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there's se_illegal instruction (0x0000) between two nop instructions (ori r0,r0,0x0). If this instruction is executed in external debug mode then debug mode is entered.

pastedImage_1.png

I tested it and it works as expected. It is necessary to set BDMEnabled to TRUE and then this code is executed at the end of function.

My question is: how did you set r1, r3 and ssd_config structure before executing the function?

Regards,

Lukas

0 项奖励
回复
7,313 次查看
kimyoungsu
Contributor III

my gpio jtag initialize sequence below.

i think go +exit function is incorrect. ??

or interrupt blocked ?

Could you give me go+exit script to run on T32?

// 1. Assert RESET
sleep_ms(10);

// 2. Set the OCMD_ENABLE_ONCE[0xFFFFFFFF]

// 3. Set the OCR[DR] and OCR[WKUP]

// 4. Deassert RESET

sleep_ms(10);

// 5. Verify debug mode via the DEBUG bit in the OnCE status register

//6. External Debug Mode Enable 

once_reg_write(bus, "OCMD_EDBCR0", DBCR0_EDM); // set EDBCR0[EDM]
once_reg_write(bus, "OCMD_DBCR0", DBCR0_EDM); // set EDBCR0[EDM]
once_reg_write(bus, "OCMD_DBSR", 0xFFFFFFFF); // clear DBSR

//7. Sram Init

//8. FMPLL init

//9. Load C55 S-Record file(i think file crc error. (???))

//10. c55_config write to sram

// 11.c55_FlashInit()

//11.1 write PC

/* no-op = e_ori 0,0,0 */
cpuscr_data.ir = 0x1800D000;
cpuscr_data.pc = data - 4;
cpuscr_data.ctl = (CPUSCR_CTL_WAITING | CPUSCR_CTL_IRSTAT8);

once_single_step(bus, cpuscr_data);

//11.2 go~~~

once_reg_write(bus, "OCMD_OCR", (OCR_WKUP | OCR_FDB));

once_ir_exec(bus, "OCMD_OSR", OCMD_READ, OCMD_GO, OCMD_LEAVE_DBG);

// 11.3 wait for Debug bit set

OCMD_NOREGSELECT read but not set debug bit so time out!!!

0 项奖励
回复
7,313 次查看
kimyoungsu
Contributor III

My ssd_config information and r1,r3 value is under picture.

is it right?

C55_SSD_CONFIG_VALUE.png

c55RegBase                           = 0xFFFE0000;
mainArrayBase                        = 0x00404000;
lowBlockInfo.n16KBlockNum  = 0;
lowBlockInfo.n32KBlockNum  = 0;
lowBlockInfo.n64KBlockNum  = 0;

midBlockInfo.n16KBlockNum  = 0;
midBlockInfo.n32KBlockNum  = 0;
midBlockInfo.n64KBlockNum  = 0;

highBlockInfo.n16KBlockNum = 0;
highBlockInfo.n32KBlockNum = 0;
highBlockInfo.n64KBlockNum = 0;

n256KBlockNum                      = 0;
uTestArrayBase                       = 0x00400000;
mainInterfaceFlag                    = 0x1;
programmableSize                   = 0x80;
BDMEnable                              = 0x01;

r1_r3.png

0 项奖励
回复
7,313 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I tested it using this config structure:

pastedImage_1.png

The BOOL is defined as "typedef unsigned char BOOL;" in ssd_types.h, so the alignment is different. Could you give this a try?

Regards,

Lukas

7,313 次查看
kimyoungsu
Contributor III

LW1wOiZr.jpg

Thank you for your reply.

I am very happy. I can go to next step.

I suffered for 3 week.

Thank you.

0 项奖励
回复
7,313 次查看
kimyoungsu
Contributor III

Thank you for your reply.

I tested for 2 things. i can entered debug mode.

t32_once_en.png

1. Write OnCE Command : 111 1110 Enable_OnCE

   1. Refer to MPC5748G Refernce Manual Rev 4, 07/2015

   2. Page 3146  section 62.8 Basic Steps for Enableing, Using, and Exiting External Debug Mode

t32_once_en_lucas.png

2. watchdog disable(my c code tested, your script modify)

    1. Assert Reset

    2. disable watchdog 

    3. set OCR[DR | WKUP]

    4. Deassert Reset

I have last problem.

I loaded at sram c55 flash firmware driver. 

I checked ok form T32 memory dump.

I wrote CPUSCR (PC 0x40000000 - 4, "no reg sel",  Go + Exit) for run FlashInit function.

That is not re-entered debug mode.

searching data sheet....... now....(EDBCR0, Access to Debug Resources, ... i don`t know how to control other register.)

MPC5646C working is good but MPC5748G working is not good. so a little different how to control.

cnre00.png

cnre.png

0 项奖励
回复