Hi,

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi,

1,474 Views
apoornak
Contributor I

Hi, 

         Few Developers faced the below issue and had posted it in here already, but have not got the answers yet. So am posting it again hoping to get an answer.

Am facing some problem when using PE-Micro MULTILINK UNIVERSAL FX to debug our product which use s MPC5744P as the controller and it was in S32DS.

 When I start debugging, the progress reaches till 98%, and the console stays infinitely with the message below:

CMD>VC

Verifying object file CRC-16 to device ranges ...

   block 00FA0000-00FA0007 ...

 But with the same project and source code this situation doesn't happen in DEVKIT.

 please lemme know the better solution than replacing the Controller Chip and what could have caused the issue.

All responses are welcomed. Especially expecting support from NXP tech team.

nxp support

nxp partner‌

using nxp community‌

Thanks in advance.

0 Kudos
Reply
1 Reply

1,405 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

this situation can be caused by legacy PeMicro debugging interface. It is always recommended to use latest S32DS updates, which contains also PeMicro debug interface updates.

For now, update 9 is the latest one. Please download and check, if the problem persist.

https://community.nxp.com/docs/DOC-342355?sr=search&searchId=53646cb0-3b84-4d77-84e9-91e4a952f9a1&se... 

Regards,

Martin

0 Kudos
Reply